Issue:
Installing branch mounted subfeed lugs into I-Line panelboards.
Product Line:
Subfeed lugs
Environment:
I-line, HCM, HCW, HCP, HCRU
Cause:
Application assistance
Resolution:
The SL1200P* kits CANNOT be installed on the narrow side of an I LINE interior. The SL800 and SL800M5 are the only subfeed lug kits that can be installed on the narrow side of an I LINE interior. The restrictions are based on the fact that there is no mounting track on the I-line mounting pan, for the SL1200P lug kits to mount on the narrow side.
Installing branch mounted subfeed lugs into I-Line panelboards.
Product Line:
Subfeed lugs
Environment:
I-line, HCM, HCW, HCP, HCRU
Cause:
Application assistance
Resolution:
The SL1200P* kits CANNOT be installed on the narrow side of an I LINE interior. The SL800 and SL800M5 are the only subfeed lug kits that can be installed on the narrow side of an I LINE interior. The restrictions are based on the fact that there is no mounting track on the I-line mounting pan, for the SL1200P lug kits to mount on the narrow side.
Released for: Schneider Electric Canada