Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Video: EcoStruxure™ Web Services (EWS) - Error: Service not enable on the server
Issue
When attempting to navigate to the EWS endpoint, the page returns an error stating "Service not enable on the server".

Service not enable on the server
Product Line
Power Monitoring Expert 8.x
Power Monitoring Expert 9.0
Power Monitoring Expert 2020

Environment
Power Monitoring Expert

Cause
EWS, EcoStruxure™ Web Services, is not enabled by default in a PME system.

Resolution
*Warning: Take backups of any files prior to modifying them. Ensure the backups are in a location that will not be overwritten (i.e. the Desktop)
  1. Navigate to the following default directory on the PME server: C:\Program Files (x86)\Schneider Electric\Power Monitoring Expert\applications\EWS
  2. Open the 'Web.config' file in Notepad.
  3. Within the 'appSettings' section of the file, find "EWSEnabled" value.
  4. Change the value  " 0" to " 1" as shown in the highlighted text.

EWSE Enabled

5. Save the notepad file.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings