Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
On an H, J, or L frame breaker, what is the minimum equipment required for serial Modbus communication on just one breaker?
Issue:
Modbus requirements for one breaker

Product Line:
Circuit Breakers

Resolution:
In order to have serial Modbus communication on an H, J, or L frame breaker, the breaker must have either an Ammeter or Energy trip unit. Besides that, the minimum equipment required depends on whether or not breaker status is desired. While there may be a variety of methods to achieve this, the below pictures shows two different scenarios:
  • Without breaker status
  • With breaker status
Graphic #1

Graphic #2

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings