Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Video: How to install LV426905 fixed ON/OFF position handle padlock attachment on the PowerPacT B frame circuit breaker (unit mount ONLY)
Issue:
How do you install the LV426905 padlock device on a unit mount B-frame breaker?

Product Line:
Molded Case Circuit Breakers

Resolution:
NOTE: This is for UNIT MOUNT B-frame circuit breakers (it is NOT for I-Line B-frame circuit breakers​)
Slide the tab on the padlock attachment into the slot above the handle on the breaker. Then, screw the attachment onto the breaker with the provided screw. For more installation information, see the attached installation bulletin.

Schneider Electric Canada

Attachment(s)
B Frame Fixed Padlock Attachments.pdf [1.46 MB]
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings