Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is the neutral assembly included with the MD motor disconnect switches?
Issue:
Is there an option to land the neutral built in to the MD3304X or MD3604X switch?

Product Line:
Digest 177 Section 8 : Operating Mechanism & Disconnect Switches

Environment:
North American Products

Cause:
Confirming if there's  an option to land the neutral built in to the MD3304X or MD3604X switch.

Resolution:
There is not a neutral assembly included. There is a provision to land the ground in this switch.
The MDS30P 30 amp add on power pole can be added and used to break the neutral.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings