How can we help you today?

Are the Terminals on the ZBV* Light Modules Polarity Sensitive?

Issue:
How should 22 mm light modules be wired, and does polarity need to be observed?

Product Line:
Push Buttons and Operator Interface

Environment:
22mm Pushbuttons

Resolution:
Most units do not need to be wired with respect to polarity.  For consistency, always land positive on X1 and negative on X2.