Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Which ION Meters are NERC CIP Compliant

Issue
Which ION meters are compatible with NERC CIP standards?

Product Line
ION meters

Environment
North American Electric Reliability Corporation (NERC).

Information about NERC can be found here.

Cause
NERC develops and enforces Reliability Standards to assure the reliability and security of the bulk power system in North America.

Resolution
At this time only the ION8650 is NERC CIP compliant.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings