How can we help you today?

PME web application is directed to settings page

Issue
PME web application goes to the 'settings' page, http://<server_name>/web/#Settings, and there does not appear to be a way to go to other tabs (dashboards, diagrams, alarms, ...).  The alarm banner is also missing.
Trying to force it to open other tabs such as http://<server_name>/web/#Diagrams doesn't help and it reverts back to the settings page.

Web Application Settings

Product Line

Power Monitoring Expert 7.2.x

Power Monitoring Expert 8.x

Power Monitoring Expert 9.0

Power Monitoring Expert 2020


Environment
Floating License Manager

Cause
Untrusted licenses:

SE Floating License Manager
This license is untrusted and has to be repaired. Reason: Backup restored.

Resolution
*Warning: During a restart of the FLEXnet License Administrator all floating licenses on this instance of the Enterprise License Server, are temporarily not available. The functionality of software products using licenses from this server may temporarily be reduced during restart.*

1. Start the Schneider Electric Floating License Manager.

2.  In the Local tab activate one or several checkboxes in the first column of the list to select the license(s) of the software product(s) to be repaired.

3.  Click the Repair button. The Repair Method dialog opens.

4.  Select a method for the repair option, for example, 'web' (if the server is connected internet).

5.  Click the Next button. A message box opens. It indicates that a restart of the FLEXnet License Administrator needs to be performed to complete the repair process.

6.  Click the Yes button to continue (or click the No button to abort).

7.  After the license is successfully repaired, click the Finish button.

Schneider Electric Canada
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
  • Contact Sales
  • Find our Offices
  • Where to Buy
  • Careers
  • Company Profile
  • Investors
  • Newsroom
  • Report a Misconduct
  • Product Documentation
  • Product Selectors
  • Software and Firmware
  • Product Substitution and Replacement
  • Blog
  • Events
  • Schneider Electric Community
  • Sustainability
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings