Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Power Monitoring Expert - PowerShell Scripts to Start / Stop ION Services

Issue:
Power Monitoring Expert does not include the functionality to quickly stop and start all of the ION services.

Product Line:

Power Monitoring Expert 9.x

Power Monitoring Expert 2020

Power Monitoring Expert 2021

Power Monitoring Expert 2022

Power Monitoring Expert 2023

Power Monitoring Expert 2024



Environment:
Windows Services

Resolution:


The PME 9 scripts are valid for PME 9.0 to PME 2020.

The PME 2023 scripts are valid for PME 2021 to PME 2023.

The PME 2024 scripts are valid for PME 2024.


The attached PowerShell scripts can be used to quickly stop and start all of the service without having to manually stop and start each one.

1) Download and save the .ps1 files to the \Power Monitoring Expert\ folder.
2) Right click and select "Run with PowerShell"

The PowerShell window will appear and then go away when the services have finished stopping / starting.

Alternatively, you can run the Powershell ISE as an admin, select File Open and then run the scripts from there.


Note: These scripts will also stop / start the ApplicationModules services as well as any custom Virtual ION Processor (VIP) services that have been created.

Schneider Electric Canada

Attachment(s)
PME9 StarStop Scripts.zip [11.2 KB]
PME2023 Services StopStart Scripts.zip [1.56 KB]
PME 2024 Services List.zip [10.42 KB]
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings