Can a mission critical circuit breaker be 100% rated?
Product Line:
Powerpact circuit breakers
Resolution:
Yes, but only the 250 A and 400 A L frame Powerpact. The 600 A L frames and the Powerpact J frames are only available in 80% rated.
Product Line:
Powerpact circuit breakers
Resolution:
Yes, but only the 250 A and 400 A L frame Powerpact. The 600 A L frames and the Powerpact J frames are only available in 80% rated.
Discuss this topic with experts
Product Resources