Issue:
What is the NEMA rating of the TVS12RMU remote monitor?
Product Line:
Surge Protective Devices (SPDs)
Environment:
Maintenance
Cause:
NEMA Rating
Resolution:
The TVS12RMU is NEMA 1 rating. NOT RATED FOR OUTDOOR USE
What is the NEMA rating of the TVS12RMU remote monitor?
Product Line:
Surge Protective Devices (SPDs)
Environment:
Maintenance
Cause:
NEMA Rating
Resolution:
The TVS12RMU is NEMA 1 rating. NOT RATED FOR OUTDOOR USE
- Intended for indoor use only.
- Use in dry locations only.
- If used outdoors, all warranties are voided and device will not function properly.
Released for: Schneider Electric Canada