Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the fingersafe rating for PowerPacT B frame breakers?
Issue:
Do PowerPacT B frame breakers have a finger safe rating?

Product Line:
Circuit Breakers

Resolution:
The standard PowerPacT B frame circuit breaker does not provide fingersafe protection.
However, when an optional long terminal shield is added to 2p, 3p, or 4p breakers, it then has a rating if IP40.
The "4" indicates protection against solid objects greater than 1mm, and "0" indicates there is no protection against liquids.
Following are the part numbers of the long terminal shields:
LV426911
LV426912
LV426913

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings