Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Connection cable of HMISTO501 to Zelio Logic
Issue:
What cable is used to connect the HMISTO501 to the Zelio Logic Relay SR2/SR3?

Product line:
HMI, Relay, PLC

Environment:
Magelis, Zelio Logic Relay, Vijeo Designer, ZelioSoft2

Resolution:
The cable to use is the SR2CBL09.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings