Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Does an Overload Relay Directly Break the Power Connections Being Passed Through it?
Issue:
Does an Overload Relay Directly Break the Power Connections Being Passed Through it?

Product Line:
Overload Relays - GIC Product

Environment:
US Product

Cause:
Product Application

Resolution:
An overload relay will never directly break the power connections running through it to the motor.  The relay is designed to open its normally closed relay contact when an overload is present.  In a standard design, this contact is run in series with the contactor coil.  When the contact opens, the coil drops out and the contactor breaks the power connections.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings