Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What are the communication ports on the CM4000 series meter and where are they located?

Issue
A customer would like to know the locations of the communication ports on a CM4000 series meter.

Product Line
CM4000, CM4000T

Environment
Communication Ports
ECC21 Card

Resolution
The following communication ports are shown on a CM4000 series meter
COM1: RS-485 (Communication with daisy-chained devices)
COM2: RS-232 (Direct communications to the PC)

If the CM4000 series meter has an ECC21 card, then the following additional communication ports are available:
COM3: RS-485 (Communication with daisy-chained devices accessible through the Ethernet gateway)
Ethernet (Modbus TCP connection)
Fiber-optic (located to the right of the Ethernet port)

CM4000 connection points

See FA203481 for more details on the ECC21's COM3 connection. The ECC21 Installation Guide is attached.

Schneider Electric Canada

Attachment(s)
ECC21_InstallationGuide_63230-304-201A3.pdf [1 MB]
Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings