Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What are the lever arms for 9007C Limit Switch that has a wide roller?
Issue:
What are the lever arms for 9007C Limit Switch that has a wide roller?

Product Line:
9007AW and 9007C Lever Arms and Special Features

Environment:
Heavy Duty Industrial Single- and Two-Pole

Resolution:
9007HA23 - 1inch wide
9007HA20 - 1 5/8inch wide
9007HA26 - 2inch wide
9007HA21 - 2 1/8inch wide

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings