Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the rebuild kit , packing for a VK-9313-372-4-12 and -13 valve
Issue:
What is the rebuild kit , packing for a VK-9313-372-4 valve 2 1/2" and 3"

Product Line:
Valves and Acuators

Environment:
Maintenance

Cause:
Replacement

Resolution:
The repair kit for the VK-9313-372-4-12 is the RYB-931-12
The 2 1/2 and 3" VB-9313 valves used a YBA-651-1 packing kit , but is now obsolete. A YBA-652-2 Packing cartridge can be used for current offering

Kit

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings