Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the terminal lug data for ALL the 60 amp, US and Canada, Heavy Duty Safety Switches (for Example: CH362, CH362DS, CHU362AWK, H362, H362DS, HU362 etc.)?

Issue:

Product Features

Product Line:
Heavy Duty Safety Switches

Environment:
Main lug terminal data

Cause:
Application

Resolution:
The standard lug wire range for the 60A heavy duty safety switches is (1) #12 - #3 (AL) OR  (1) #14 - #3(CU).

NOTES:
1) 30 -100 A switches are suitable for 60 or 75 degree wires. EXCEPT the H60XBD and H60XBDAA use 75 degree CU wire ONLY. Use #6 AWG Copper Wire MAXIMUM for 60Amp Rating.
2) There are NO alternate lugs available, other than compression lugs and the compression lugs DO NOT allow for larger or more wires. See the Switch Wiring diagram or current On-Line Digests for Compression lug part numbers.


Schneider Electric Canada
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
  • Contact Sales
  • Find our Offices
  • Where to Buy
  • Careers
  • Company Profile
  • Investors
  • Newsroom
  • Report a Misconduct
  • Product Documentation
  • Product Selectors
  • Software and Firmware
  • Product Substitution and Replacement
  • Blog
  • Events
  • Schneider Electric Community
  • Sustainability
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings