Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is part number 31051-014-01?
Issue:
What is the replacement for part number 31051-014-01

Product Line:
9001 type K and SK 30 mm Push Buttons

Environment:
Harmony 30mm

Cause:
Product Selection

Resolution:
This is a nylon liner on the back of some 9001 type K and SK switches it is not available as a replacement part, the operator itself will need to be replaced.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings