Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What are the coil characteristics of the LXD3G7, LXD3LE7, LXD3W7, and LXD3T7 coils?
Issue:
Identify the coil characteristics of the LXD3G7, LXD3LE7, LXD3W7, and LXD3T7 coils

Product Line:
IEC Contactors - GIC Product

Environment:
US Product

Cause:
Product Specification

Resolution:
The LXD3G7, LXD3LE7, LXD3W7, and LXD3T7 are coils designed specifically for the US market and are different in characteristics from the other LXD3 coils available:
LXD3G7 - 120V 60hz only with a tolerance of -15% and +10%.  Inrush 200VA and holding 19VA
LXD3LE7 - 208V 60hz only with a tolerance of -15% and +10%.  Inrush 200VA and holding 19VA
LXD3W7 - 277V 60hz only with a tolerance of -15% and +10%.  Inrush 200VA and holding 19VA
LXD3T7 - 480V 60hz only with a tolerance of -15% and +10%.  Inrush 200VA and holding 19VA

Schneider Electric Canada

Explore more
Product:
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings