Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How can the isolation contactor be engaged on the Altistart ATS22 soft starter without tripping the PHF error code?

Issue:

Isolation contactor engagment on the ATS22 without tripping on PHF faults

Cause:
Application has no time delay timer.

Resolution:
Set  r1/ r2  to trip . You must applied control voltage before the run command is given.
Note: trip settings allow the relay to energize on control voltage power up.

***

If this article does not answer your question, check out our FAQ database that has answers to more commonly asked questions: Frequently Asked Questions - Schneider Electric (se.com)

If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance: Support | Schneider Electric Global (se.com)

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings