How can we help you today?

What are the bolt hole center line dimensions for the flanges used on a VB-9XXXX Series Valves?

Issue:
What are the dimensions for bolt hole center line on the flanges used on a VB-9XXXX Series Valves?

Product Line:
Valves and Actuators

Environment:
Installation

Cause:
Clarification

Resolution:
For the VB-9XXX Series Valves, use the  "C" Centerline dimensions /per Pipe size listed below

The below image is listed in all the VB-9000 series valve documents


Bolt Pattern Dimensions

Schneider Electric Canada

Attachment(s)
VB-9000 2-way .5 inch - 6 inch Dimensions.pdf [55.2 KB]
VB-9000 3-way .5 inch - 6 inch Dimensions.pdf [49.45 KB]