Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can the H60FXA , Nema 7/9 enclosed, Automatic Molded Case switch be ordered for 30 A.
Issue:
Can the fuses be switched out to 30A for the H60XFA switches?

Product Line:
Safety Switches

Environment:
Application

Cause:
Product Features

Resolution:
The H60XFA switch has a molded case switch and not fuses. The smallest amperage for the Hazardous Duty switches is 60A . It is also available in the N7/9 enclosure with 100A, (H100XFA) and 225A (H225XJG) .

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings