Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the rated conductivity of NQ panel with aluminum bus?
Issue:
What is the rated conductivity of NQ panel with copper bus?

Product Line:
panel

Environment:
NQ panel

Resolution:
Aluminum in NQ panels have 56.5% conductivity and the copper is 96%.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings