Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How are the dials on the REXL relays set?

Article available in these languages: Japanese

Issue:
How do we set the REXL timing range?

Product Line:
Relays and Timers

Environment:
All Products

Cause:
Installation and Setup

Resolution:
On the REXL we feature two dials. The dial settings are as follows:

Dial 1: The dial on the bottom of the relay is a 7-position timing range selector:
(0.1-1 s)         (1-10 s)        (0.1-1 min)
(1-10 min)      (0.1-1 h)       (1-10 h)
(10-100 h)
Dial 2: The dial on the front of the relay is the selection for adjustment of the time
delay, graduated in % of range max.

To set the Adjustment of the Time Delay:
  • Select the timing range immediately greater than the time required, using dial 1
  • Using selector dial 2, select  the required timing value as a % of setting on switch 1.
For example: if the timing range required is 30 minutes we would set dial 1 to .1-1h, and dial 2 to 50%

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings