Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can additional contact block be added on the Cover-Mounted Hand-Off Auto Switch on a NEMA FV Starters and Contactors?
Issue:
Additional contact block part number for HOA kit 9999SC2 and 9999SC9

Product Line:
NEMA and Definite Purpose Contactors and Starters

Environment:
Class 8502 & 8536, 8538, 8539, 8702, 8736, 8903 (Electrically Held)

Resolution:
For the cover-mounted control unit kit 9999SC2 which is a rectangular Hand Off Auto selector switch, additional contact blocks CANNOT BE ADDED. On the other hand, for the NEMA 4/4X Kit 9999SC9 which uses a 9001 SKS43B - 3 position selector switch, a  9001KA1 - Contact block CAN BE ADDED.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings