Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the part number for hook stick, temporary ground cables and primary grounding bars for Metal Clad VR Manual Ground and Test Device?
Issue:
What is the part number for hook stick, temporary ground cables and primary grounding bars for Metal Clad VR Manual Ground and Test Device?

Product Line:
Metal Clad Switchgear

Environment:
Replacement parts

Cause:
Ordering

Resolution:
Assemblies for grounding bars are listed for 5/15kV and 27kV :
(1) 46002-513-04 HOOKSTICK SER 2,3 &5 MGTU #8104 LEN 4' 6"LONG
(1) 46002-517-50 EYEBOLT GRD CBL ASSY S2-5 HASTINGS (1) Ground cable supplied
(1) 46007-186-50 BAR GRD ASSY SER 5 MGTU  5KV
(1) 46027-920-50 BAR GRD ASSY SER 5 MGTU 27KV
hook stick

Schneider Electric Canada

Attachment(s)
VR Ground and test device 6055-42.pdf [945.81 KB]
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings