Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the part number of the body unit with top cover for XVU Illuminated LED Units?
Issue:
What are the voltage range of the body units for an XVU tower lights?

Product Line:
XVU 60 mm Diameter Tower Lights and Beacons

Environment:
Tower Lights and Beacons

Resolution:
The body unit with top cover comes in two voltages, 24V and 100-240V. For the 24V it is, XVUC21B for Black and XVUC21BQ Silver.  For 100-240V XVUC21MP for Black and XVUC21MQP (Obsolete).

Schneider Electric Canada

Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
  • Help and Contact Center
  • Contact Sales
  • Find our Offices
  • Where to Buy
  • Careers
  • Company Profile
  • Investors
  • Newsroom
  • Report a Misconduct
  • Product Documentation
  • Product Selectors
  • Software and Firmware
  • Product Substitution and Replacement
  • Blog
  • Events
  • Schneider Electric Community
  • Sustainability
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings