Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How do you find the IP address for an IFE?
Issue:
What is the IP address for a circuit breaker connected to an IFE module?

Product Line:
Circuit Breakers

Resolution:
By default, the first two sets are always 169.254. The next two sets are on a label on the IFE written in HEX format, which must be converted to decimal. As an example, if a label on an IFE is "IFE-E3.AB.7C", AB converts to 171, 7C converts to 124, so the complete IP address is 169.254.171.124.

Schneider Electric Canada

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings