Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is part number 45XB377-1?
Issue:
The labeled number does not come up as a Schneider part number

Product Line:
Panelboard Lighting Contactors

Environment:
NEMA Contactors and Starters

Resolution:
This is the manufactures part number on the bridge rectifier in Class 8903 Type PB (panelboard) lighting contactors.  We sell this under the Schneider part number 31155-025-01.  It is 1.25" square with 1/4" spade type slip-on terminals and a .20" mounting hole in the middle.  It is rated 2KV (max peak reverse voltage),

Schneider Electric Canada

Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
  • Help and Contact Center
  • Contact Sales
  • Find our Offices
  • Where to Buy
  • Careers
  • Company Profile
  • Investors
  • Newsroom
  • Report a Misconduct
  • Product Documentation
  • Product Selectors
  • Software and Firmware
  • Product Substitution and Replacement
  • Blog
  • Events
  • Schneider Electric Community
  • Sustainability
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings