Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is it possible to use different voltages on the field side of an Telefast ABE- 7P16F310?
Issue:
Does the Telefast ABE-7P16F310 allows for different voltages to be used on the field side of the module?

Product Line:
Telefast, Modicon, Telemecanique

Environment:
PLC, Interfacing relay

Resolution:
Yes you can use different voltages on the field side of the module. The voltage to be used will be determined by the solid state plug in module used. Here is a list of the available modules:

ABS-7EC3AL (5 VDC TTL)
ABS-7EC3B2 (24 VDC)
ABS-7EC3E2 (48 VDC)

ABS-7EA3E5 (48 VAC)
ABS-7EA3F5 (110/130 VAC)
ABS-7EA3M5 (230/240 VAC)

Schneider Electric Canada

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
  • Help and Contact Center
  • Contact Sales
  • Find our Offices
  • Where to Buy
  • Careers
  • Company Profile
  • Investors
  • Newsroom
  • Report a Misconduct
  • Product Documentation
  • Product Selectors
  • Software and Firmware
  • Product Substitution and Replacement
  • Blog
  • Events
  • Schneider Electric Community
  • Sustainability
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings