Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the part number of the replacement overload on GV2 or GV3 starters?
Issue:
Are internal parts of the GV2 and GV3 starters replaceable ?

Product Line:
IEC Contactors and Starters

Environment:
TeSys GV Manual Starters and Protectors

Resolution:
The overload portion of the GV2 starters and all internal parts are not replaceable. Need to replace the whole starter once damage.  The only replaceable part is the auxiliary contacts.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings