Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can the B-frame breakers be used on delta systems?
Issue:
Are there any B-frame circuit breakers that are rated for delta voltage systems?

Product Line:
Powerpact Molded Case Circuit Breakers

Resolution:
The 600Y/347 V rated B-frame circuit breakers (e.g. BGL36100) are rated for use on 240 Vac and 480 Vac delta voltage systems. None of the B-frames are rated for use on 600 Vac delta voltage systems.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings