Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the wire type and temperature rating for Tesys D contactors?
Issue:
Customer wants to use 90C rated wires. Wants to know if they can use this on the LC1D contactors.

Product line:
IEC Style Tesys D, LC1D Contactors

Environment:
IEC Contactors and Starters

Resolution:
All IEC contactors were tested and UL listed for use with 75 Degree Celsius copper wires only for the Power circuit. The product will list this information, in addition to the instruction bulletin (see attached)
They can use 90C rated wires, but must rate these per the 75C charts in the NEC guide.

Schneider Electric Canada

Attachment(s)
D09_D38 IB 1378323_ 01A55-11.pdf [776.8 KB]
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings