Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is it possible to use a three phase load center for a single phase application?
Issue:
Three phase load center for single phase application

Product Line:
Load Center

Resolution:
It is not possible for three phase load centers to be used for single phase because it would be considered a violation of NEC.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings