Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Where to find information about HomeLine Fusible Loadcentre Inserts (HFLCI)

Issue:

The customer wants to replace old fusible Loadcentre  with breaker Inserts

Product Line:
Canadian HomeLine™ Loadcentres

Environment:
Products sold and used in Canada

Cause:
Reducing  installation time, as much as 80%, allowing for the economical replacement of old fusible loadcentres.

Resolution:
READ THIS FIRST!

To select the proper HFLCI, follow these three steps using the attached file:
Step 1: Find your fusible loadcentre catalogue number using columns 1 and 2.
Step 2: Confirm that the original fusible loadcentre box dimensions match those in columns 5, 6, and 7.
Step 3: Use column 3 to identify the HomeLine Fusible Loadcentre Insert (HFLCI) catalogue number

Schneider Electric Canada

Attachment(s)
HFLCI.pdf [62.98 KB]
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings