Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the weathershield for transformers in a size 25J enclosures to make them suitable for outdoor applications?
Issue:
Is there a weather shield for transformers in a type 25J enclosure to make them suitable for Nema 3R applications?

Product line:
Transformers

Environment:
Low Voltage General Purpose, Dry Type Transformers

Resolution:
The weather shield part number 7400WS25J, can be used for the enclosure openings to provide a Nema 3R rating to the Transformer.

Schneider Electric Canada

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings