Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What are the flying lead cable options for the BMXDDM3202K
Issue:
Are there pigtail cables for the BMXDDM3202K.

Products:
X80, M340, M580

Resolution:

For flying lead (Pigtail) you can use cables:
BMXFCW303  3m
BMXFCW503  5m
BMXFCW1003  10m

Schneider Electric Canada

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings