Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Video: How to configure the PM8000 digital inputs using ION Setup

Issue
Configuring Digital Input parameters of PowerLogic PM8000 series power meters via ION Setup.

Product Line
PM8000 series meters

Environment
ION Setup
User guide, Meter configuration, Digital Inputs

Cause
Need to know how to configure the digital inputs on a PM8000 using ION Setup

Resolution
You can use ION Setup to configure the meter's onboard and/or option module digital inputs.

To configure the onboard digital inputs using ION Setup:

  1. Start ION Setup.
  2. Open the Setup Assistant for your meter.
  3. Navigate to I/O > Digital Inputs. The tabs correspond to each digital input. Click on the tab for the digital input you want to edit.
  4. Configure the digital input by selecting the parameter and clicking Edit.
  5. Once the parameter has been configured, click OK to save the setting to the meter.
ParameterValue/rangeDescription
Input ModePulse, KYZ, A/C, IRIG-BSpecifies how the meter processes the signal:
  • Pulse: the meter counts an entire pulse (from off-on to on-off) as one input.
  • KYZ: the meter counts a transition (from off-on to on-off) as one input.
  • A/C: the meter detects analog signals where the ON condition is based on the presence of an AC signal.
  • IRIG-B: the meter detects an IRIG-B time synchronization signal.
PolarityInverting/Non-invertingSpecifies if the signal from the digital port is inverted or not inverted.
Debounce0.000 - 1.000Specifies how long (in seconds) the signal must remain in a state to be considered a valid state change.
PortDefined by your meter's hardwareYour meter's physical digital input port.


Note: IRIG-B can only be connected to one of the digital inputs located on the meter base, not an option module. You must also configure your meter's clock to use IRIG-B time synchronization.


To configure the option module digital inputs using ION Setup:

  1. Start ION Setup.
  2. Open the Setup Assistant for your meter.
  3. Navigate to Expansion Module > Option I/O Modules and select the module tab that corresponds to the option module with the digital input you want to configure.
  4. Select the digital input channel and click Edit. The setup screen for that digital input is displayed.
  5. Configure the digital input by selecting the parameter and clicking Edit.
  6. Once the parameter has been configured, click OK to save the setting to the meter.
ParameterValue/rangeDescription
Input ModePulse, KYZ, A/C, IRIG-BSpecifies how the meter processes the signal:
  • Pulse: the meter counts an entire pulse (from off-on to on-off) as one input.
  • KYZ: the meter counts a transition (from off-on to on-off) as one input.
  • A/C: the meter detects analog signals where the ON condition is based on the presence of an AC signal.
  • IRIG-B: the meter detects an IRIG-B time synchronization signal.
PolarityInverting/Non-invertingSpecifies if the signal from the digital port is inverted or not inverted.
Debounce0.000 - 1.000Specifies how long (in seconds) the signal must remain in a state to be considered a valid state change.
PortDefined by your meter's hardwareYour meter's physical digital input port.


Note: IRIG-B can only be connected to one of the digital inputs located on the meter base, not an option module.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings