Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the replacement Open/Close indicator for a Medium Voltage Vacuum Breaker V5D4122Y000?
Issue:
Can the Open /Close indicator be replaced in a current VR medium voltage breaker ?

Product Line:
Metal Clad Switchgear

Environment:
Maintenance

Cause:
Replacement

Resolution:
The complete breaker mechanism must be replaced for a damaged open/close indicator.  The part number for the mechanism is 46040-550-50
mvvb

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings