Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the replacement part number for the "Open/Close" indicator of Medium Voltage VR Vacuum Breaker V5DXXXXXXXX?
Issue:
VR breaker Open and Close status part broke, can it be replaced ?

Product Line:
Metal Clad Switchgear

Environment:
Maintenance

Cause:
Replacement

Resolution:
The Open / Close indicator cannot be replaced by itself, it's apart of the Breaker mechanism. The complete breaker mech must be replaced when damaged open/close indicator needs replacing .
Order part 46040-550-50 for mechanism assembly

indicator

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings