Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Why would a LC1F115 chatter with a new LX1FF110 coil?
Issue:
Identify the cause why the LC1F115-F225 would chatter with a new LX1FF coil

Product Line:
Tesys F Contactors and Starters

Environment:
IEC Contactors and Starters

Resolution:
They have changed the magnet in the LC1F115 contactors and the LX1FF coils will no longer work. The existing LX1 type 50Hz or 60Hz coils cannot be used in contactors with Zinc coating magnets. LX9, LX4 and LXE coil types shall be used along with these new type magnets. Suitable marking are made on the product for the easy understanding of users. All new contactors manufactured with /without coil will be with Zinc coated magnets only.
See the attached Product information. It also lists the new coil part numbers.

Schneider Electric Canada

Attachment(s)
EN F Contactors - Zinc coating on F115-F225 Contactor magnet_L2.4.pdf [767.29 KB]
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings