Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Why can't I get my M580 X80 Ethernet drops online?
Issue
When trying to commission the M580 ERIO using BM*CRA312*0 modules, they will not communicate.

Product line
Unity Pro, Modicon M580

Resolution
One very common reason is that the incorrect CRA adapter was selected in the Unity Project. Make sure that not only the part number matches between the hardware and project but also the firmware revision.

The next top reason is the switch settings. The switches can be finicky. Try rotating a full 360 to 0 then counting indents.

If you have been altering module Ip addresses to match your network, create a scratch configuration and just map the CRAs using default addresses and test with that project to distinguish between a hardware or software issue. All that you need configure is the CPU and CRA modules, nothing else.

Schneider Electric Canada

Attachment(s)
Selecting X80 IO adapters.jpg [212.96 KB]
Explore more
Product:
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings