Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Are CAD drawings available for the 9001KYSS enclosures?
Issue:
Customer is asking for CAD drawings for the 9001KYSS1 and 9001KYSS3

Product line:
Push Buttons and Operator Interface

Environment:
9001 control stations

Cause:
No CAD files online

Resolution:
CAD drawings are not available for the 9001KYSS series enclosures.  We have a single drawing available with a photo of the 9001KYSS3, 3 hole unit.  However the dimensions for all the other sizes are listed in the attached table of the drawing.

Schneider Electric Canada

Attachment(s)
9001KYSS srawing 30426-455-5x.pdf [147.89 KB]
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings