Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
ION8650 data update/refresh rate
Issue
The rate of data update in ION meters

Product Line
ION8650

Environment
ION meter advanced setup

Cause
The data update or refresh rate varies depending on whether a high or a low-speed module is under consideration.

Resolution

The ION meters have both high-speed and low-speed standard ION modules. For example, an HS power meter module is a high-speed ION module that updates data every half cycle, i.e 10 ms. Whereas, standard ION modules like Arithmetic module, Analog out module or Alert module, they are slow speed modules and update data every 1 second.

If you link a standard ION module to a high-speed ION module, the update rate is determined by the slower module. To take advantage of the fast update rate, only choose high-speed modules in your high-speed framework. The number of high-speed modules is limited, so use them only when necessary.

Also, a high-speed ION module like HS power meter module can be used to send data to an external SCADA system, provided that SCADA system can manage the update rate of 1 second.

The protocol DNP can update at the 1/2 cycle rate, but only for a few measurements as configuring the module for 1/2 cycle uses a significate amount of CPU power.

Schneider Electric Canada
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
  • Contact Sales
  • Find our Offices
  • Where to Buy
  • Careers
  • Company Profile
  • Investors
  • Newsroom
  • Report a Misconduct
  • Product Documentation
  • Product Selectors
  • Software and Firmware
  • Product Substitution and Replacement
  • Blog
  • Events
  • Schneider Electric Community
  • Sustainability
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings