Video: How to install the 9999SP2R Pilot Light Kit for NEMA starters?
Issue:
Installing 9999SP2R Pilot Light Kit in NEMA 1 Type S Starters
Product Line:
NEMA and Definite Purpose Contactors and Starters
Environment:
NEMA starter accessories
Resolution:
9999SP2R is designed for use with NEMA Size 00 to 3, Type S Class 8502 contactors and Class 8536 starters mounted in NEMA 1 general purpose enclosures with slip-on covers.
The pilot light kits can be used on any voltage through 600 V, 50 or 60 Hz. The pilot lights indicate when the contactors or starters are energized.
Please refer to following video and Instruction Bulletin #30072-003-36 for the step by step instructions for the installation of this pilot light kit.
Installing 9999SP2R Pilot Light Kit in NEMA 1 Type S Starters
Product Line:
NEMA and Definite Purpose Contactors and Starters
Environment:
NEMA starter accessories
Resolution:
9999SP2R is designed for use with NEMA Size 00 to 3, Type S Class 8502 contactors and Class 8536 starters mounted in NEMA 1 general purpose enclosures with slip-on covers.
The pilot light kits can be used on any voltage through 600 V, 50 or 60 Hz. The pilot lights indicate when the contactors or starters are energized.
Please refer to following video and Instruction Bulletin #30072-003-36 for the step by step instructions for the installation of this pilot light kit.