Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is it possible to convert an 8538 size 0 combo starter to a size 1?
Issue:
What is needed to convert a size 0 8538 combo starter to a size 1?

Product line:
Class 8538 and 8539 Type S combination starters

Environment:
Products sold in North Amreica

Resolution:
Yes, its possible since size a 00 to size 1 8538/8539 combo starter they have the same base plate and bigger than that it's going to be separate mount. Needs to change the contactor part with the same coil voltage.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings