Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Video: What is included in the 9999SX8 and how to install it?
Issue:
Installing 9999SX8 Auxiliary Contact Kit in NEMA 1 Type S Starters

Product Line:
NEMA and Definite Purpose Contactors and Starters

Environment:
NEMA Type S accessories

Resolution:
The 9999SX8 is an auxiliary contact kit for field mounting auxiliary contacts to Size 00-7 contactors or starters. It includes 1 N.O and 1 N.C. auxiliary contact which is field convertible from N.O. to N.C. or from N.C. to N.O.

Please see the following video and the Instruction Bulletin #30072-013-21 for the un-boxing and step by step installation guide.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings