Where Can I Get The Instruction Bulletin for the NEMA Size 2 8502/8536 Type SD Contactors and Starters?
Issue:
Instruction bulletin to get the component part numbers for the 8502SD* and 8536SD* devices
Product Line:
NEMA Contactors and Starters
Environment:
8502/8536 Contactors and Starters
Resolution:
The attached files are for SERIES A Starters Class 8502/8536, using the melting alloy or solid starter overload relay.
File name 30072-013-24 using the solid state overload relay
File name 30072-013-11 using the melting alloy overload relay
Instruction bulletin to get the component part numbers for the 8502SD* and 8536SD* devices
Product Line:
NEMA Contactors and Starters
Environment:
8502/8536 Contactors and Starters
Resolution:
The attached files are for SERIES A Starters Class 8502/8536, using the melting alloy or solid starter overload relay.
File name 30072-013-24 using the solid state overload relay
File name 30072-013-11 using the melting alloy overload relay
Released for: Schneider Electric Canada




Need help?
Product Selector
Quickly and easily find the right products and accessories for your applications.
Get a Quote
Start your sales inquiry online and en expert will connect with you.
Where to buy?
Easily find the nearest Schneider Electric distributor in your location.
Help Center
Find support resources for all your needs, in one place.