Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Where Can I Get The Instruction Bulletin for the NEMA Size 3 8502/8536 Type SE Contactors and Starters?
Issue:
Instruction bulletin to get the component part numbers for the 8502SE* and 8536SE* devices

Product Line:
NEMA Contactors and Starters

Environment:
8502/8536 Contactors and Starters

Resolution:
The attached files are for SERIES A Starters Class 8502/8536, using the melting alloy or solid starter overload relay.

File name 30072-013-25, 3-pole using the solid state overload relay
File name 30072-013-01, 2 & 3 poles using the melting alloy overload relay
File name 30072-013-03, 4 & 5 poles using the melting alloy overload relay

Schneider Electric Canada

Attachment(s)
30072-013-01.pdf [142.14 KB]
30072-013-25.pdf [237.14 KB]
30072-013-03.pdf [148.73 KB]
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings